AXIS#.MOTOR.IDDATAVALID

Description

AXIS#.MOTOR.IDDATAVALID reports the status of the motor memory status.

The valid values for this keyword are the following:

Value

Description

0

Error in identification

1

Success in identification

2

Identification in process

3

Identification not started yet

4

Success recognizing feedback, but failed to varify OEM data integrity

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

N/A

Range

N/A

Default Value

0

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.IDDATAVALID

500bh

2dh

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6205

1

6205 (0x183d)

AXIS1.MOTOR.IDDATAVALID

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.MOTOR.IDDATAVALID

6205

Unsigned8

Read Only

-